Skip to main content
Associate
Nov 5, 2025 9:18 AM UTC
Question

DSI Video Mode (RGB888) with ST7703 on STM32U5G9NJ

 

  • uC – STM32U5G9NJH6Q

  • Display – 720 × 720 (ST7703 panel)

  • Display controller – ST7703

  • MIPI lanes – 2 lanes

  • DSI Host Mode – Video Mode (DSI_VID_MODE_BURST)

  • Pixel format – RGB888

Problem / Symptoms

  1. After the initial display setup (LP mode initialization sequence), the backlight turns ON, but no image is displayed on the LCD.

  2. I have verified that the MIPI DSI clock and data line waveforms are present and active on the scope — both lanes appear to be toggling correctly.

  3. Despite proper DSI signal activity, the panel remains blank (black screen), and there is no visible frame output from TouchGFX.

What I have verified/working

  • I can communicate with the display over DSI and run the initialization sequence (LP command mode) — panel responds, backlight comes on.

  • LTDC timings & basic parameters match the panel spec and st7703.c values (see below).

  • PHY frequency configured around panel-recommended range (450–510 MHz / VCO ~800 MHz–1 GHz).

  • TouchGFX / display driver configured to disp_ltdc. dma_2d and gpu2d acceleration enabled. vsync source set to LTDC.

  • Backlight PWM and reset GPIO working.

My LTDC configuration (current)

  • Resolution: 720 × 720 (active) — matches ST7703.

  • Pixel Format: RGB888.

  • Porch & sync (approx / set to values close to st7703.c):

    • HSync = 6, HBP ≈ 51, HFP ≈ 51 (I used HSync=6, HBP=3 earlier while calculating HorizontalLine = 1452 — verified active + porches match).

    • VSync = 2–3, VBP ≈ 12, VFP ≈ 12–15.

  • Layers: 1. Buffering strategy: Single at present (I can switch to double).

DSI Host settings

  • Mode: DSI_VID_MODE_BURST (continuous video).

  • Lanes: DSI_TWO_DATA_LANES.

  • LP command mode: enabled (to send DCS commands like DISPLAY ON).

  • PHY frequency: set to panel-recommended range.

  • LP mode enabled for porch/sync intervals (low power during those phases).

  • HorizontalLine computed appropriately for active + porches + sync (e.g. ~1452 for current timing).

TouchGFX

  • Display interface: disp_ltdc.

  • Buffering: Single (considering Double).

  • Hardware accel: dma_2d, gpu2d_enabled.

  • VSYNC source: vsync_ltdc.

Backlight / Reset

  • Backlight PWM: TIM15_CH2 on PB15 — works.

  • LCD_RESET: PD4 — matches st7703.c.

 

Has anyone successfully run TouchGFX with DSI Video Mode (burst) on an ST7703 panel (RGB888 / 2-lane)? If yes, could you share example project or configuration highlights?

 

 

This topic has been closed for replies.