Skip to main content
DPfei.16
Associate II
August 28, 2019
Question

DSI Clock Frequency

  • August 28, 2019
  • 5 replies
  • 2217 views

Hello,

i have 25 MHz HSE Clock.

The DSI PLL settings are as follows: IDF 5, NDIV 80, ODF2

With these settings i measure an DSI clock of 100 MHz on the DSI_CKP pin.

But Cube says that the DSI clock is 200 MHz.

I use a STM32F769NI device with 2 DSI data lanes.

Do you have any idea?

BR

Daniel

This topic has been closed for replies.

5 replies

Tesla DeLorean
Guru
August 28, 2019

They do on the surface look like appropriate numbers for a 200 MHz pixel clock.

As I recall the DSI clocks on both edges, effectively doubling the bandwidth, ie 100 MHz clock on pin equates to 200 Mbps on the wire.

I built a decoder for the LTDC/DSI clocks, will have to dig that up.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
DPfei.16
DPfei.16Author
Associate II
August 29, 2019

Hi Clive,

thank you for your response!

I know DSI uses double data rate (DDR) and therefore data is transfered on the rising and the falling clock edge. This means when I have a DSI clock frequency of 200 MHz I have a bandwitdth of 400 Mbit/sec.

But I don't understand why the measured DSI clock frequency is only the half of the calculated DSI clock frequency.

Tesla DeLorean
Guru
August 29, 2019

The STM32's unit clocks at 200 MHz internally so it can generate data on both edges of the 100 MHz clock on the wire.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
DPfei.16
DPfei.16Author
Associate II
September 3, 2019

Hi Clive,

many thanks for your help!

BR

Daniel