Associate II
Jul 1, 2016 3:03 PM UTC
Question
Driving TFT-LCD on STM32Fx with HAL
- 1 reply
- 1217 views
Posted on July 01, 2016 at 17:03
Hello guys,
I am using Keil Uvision 5.2 and cube Mx for developing STM32 MCUs.and I want to Drive a TFT-LCD which the size is 2.8 inch and it has 320*240 pixels and it has ILI9328 driver inside.I have few information about driving this LCDs such as it has different modes for driving such as 8-bit parallel driving, 16bit parallel driving and SPI mode.and I found some libraries for driving this LCD but that is not clear to use and uses CMSIS drivers.could anybody helpd me optimizing this library for HAL and STM32Fx MCU and using FSMC.I really need this library please.!!!!:Dthank you #hal #lcd #cubemx #tft #keil