Skip to main content
FDigi
Associate III
August 5, 2020
Solved

Does TouchGFX support the STM32H743IIT6?

Hello everyone,

I'm in the community and I started to study the STM32H7 microcontroller familly and the TOUCHGFX. After reading a few post here i discovered that there are some microcontroller the are not suppported by the TOUCHGFX enginne (apparently all the DUAL CORE MCU). If so, I would like to confirme if the STM32H743IIT6 if supported by the TOUCHGFX.

Bruno

This topic has been closed for replies.
Alexandre RENOUX
Alexandre RENOUXBest answer
Visitor II
September 8, 2020

Hello,

The H743 is supported by TouchGFX. Also the H747 is supported (even though dual core) but you cannot use CubeMX with it.

If you take a look at the different Application Templates available in TouchGFX Designer you will see that we have a complete project for the H743-EVAL board.

/Alexandre

1 reply

Alexandre RENOUX
Alexandre RENOUXBest answer
Visitor II
September 8, 2020

Hello,

The H743 is supported by TouchGFX. Also the H747 is supported (even though dual core) but you cannot use CubeMX with it.

If you take a look at the different Application Templates available in TouchGFX Designer you will see that we have a complete project for the H743-EVAL board.

/Alexandre