Skip to main content
pmv
Visitor II
Feb 27, 2019 9:08 AM UTC
Question

Does TouchGfx currently has support for i.MX6 UL board? I need to develop application screen which has to be run on imx6ul board.

..

This topic has been closed for replies.

2 replies

Mon2
Senior III
Feb 27, 2019 12:48 PM UTC

No. Do not believe so. TouchGFX (formerly Draupner product and now owned by ST) is strictly for the STM32 CPU targets.

Martin KJELDSEN
Principal III
Apr 3, 2019 10:41 AM UTC

Hi @pmv​,

Besides the truths that @Mon2​ are posting, I thought i'd just add something to this.

TouchGFX 4.10.0 and onwards are STM32 locked. Prior to that, they're not. That being said, the port for IMX6UL was always unofficial and just something i had running at my desk running Yocto Linux, so you won't find any support through the designer even if you're using an old version.

Best regards,

Martin