Skip to main content
kD1
Associate II
Aug 6, 2020 6:31 AM UTC
Question

Does B-LCD40-DSI1 display on 32F769IDISCOVERY works with one lane.

  1. I have used TouchGFX tool and implemented HMI where the configuration is with 2 lane. Now i want to work with single lane DSI configuration on 32F769IDISCOVERY to B-LCD40-DSI1 Display. Does this works ?
  2. I have my own circuit designed by considering reference schematic from 32F769IDISCOVERY. Now i shall place New display with single lane DSI feature how could i validate DSI comm is correct or wrong. The issue might be hardware else software so how can i validate, is there any tool to test software is correct ?

Regards,

Kishore D

This topic has been closed for replies.

8 replies

MM..1
Super User
Aug 6, 2020 8:14 AM UTC

When your display refresh and resolution dont exceed 500Mbit one lane then you can use it.

kD1
kD1Author
Associate II
Aug 6, 2020 12:42 PM UTC

Hi,

    32F769IDISCOVERY - HMI is generated by TouchGFX 4.13 tool. I'm able to view GUI on LCD display on two data lanes using TouchGFX tool,  but the same project I have changed two lane to One lane & LTDC pixcel clock to 20.83 as [ 500/24 ] LTDC clock source. There is no response in screen after flashing.

if any example code on 32F769IDISCOVERY to B-LCD40-DSI1 of single lane please send me.

Regards,

Kishore D

MM..1
Super User
Aug 6, 2020 6:06 PM UTC

Try use lower pixel clock and some display drivers need set register init to use only one lane.

ELee.9
Associate II
Jan 18, 2023 6:12 AM UTC

Hi, I'm really interested in this topic.

Did you finally work sucessfully using one data lane with B-LCD40-DSI1?

I finally worked in one data lane in Low Power Mode, but still not working in High Speed Mode.

Could you please tell me how to do?

Thanks.