Skip to main content
ali_dehbidi
Associate III
July 15, 2021
Question

Do you recommend TocuhGFX @ 1024x600 pixels

Hi,

I want to use STM32H750XBH6 part with a LCD of 24bit @1024x600 resolution, Do you have any Idea about the performance? is it slow or can it do the job?

This topic has been closed for replies.

4 replies

ktrofimo
Senior III
July 15, 2021

I do have now H743 @480MHz with 32bit SDRAM @133MHz​. With RGB565 I have a feeling it is just at the edge of performance. Sometimes I see glitches and I can eliminate them only by simplifying screen layout. SDRAM is fast enough (I was successful even in 16bit bus mode)

Tesla DeLorean
Guru
July 15, 2021

1024x600 @ 60 Hz 24-bpp gets pretty close to the DSIHOST bandwidth ceiling.

Are you sure you need 24-bit? Lot of pins, and +50% of the bandwidth of 16-bit

Pixel clock around 40 MHz as I recall, at 60+ MHz you're probably close to the top end of the resolutions drivable by the STM32 MCU, would really want 32-bit wide SDRAM path, especially for concurrent operation with SDMMC or DCMI

H750, probably most code in QSPI, cache will mask a lot of that, but still an underlying bottleneck, and not sure how it impacts latency and contention.

Hopefully one of the TouchGFX crew has some handy performance slides..

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
ali_dehbidi
Associate III
July 15, 2021

ktrofimo did you use 1024x600 pixels @ 16Bit? Also did you use some widgets like analog clock, graph and Date Picker?

What about putting the application code into the SDRAM too, so the QSPI is not a bottleneck. Also using the 32bit SDRAM.

ktrofimo
Senior III
July 15, 2021

I would NOT recommend to use SDRAM for any other purpose besides video buffer. Concurrent access to the SDRAM bus during frame draw by LTDC will produce ​flickering and artifacts.

Widgets - yes, analog clock, dynamic graph in scroll mode with filled semi-transparent area under the line, dozen text fields updated several times per second...​