Skip to main content
Öyild.1
Associate II
August 16, 2021
Solved

Displaying integer variable problem for STM32F429-DISCO

I am using STM32F429-DISCO developer board and I am following this tutorial. I got two buttons for increasing and decreasing an integer counter.I would like to display this variable on screen. I applied all the steps but I got "?" icon when I push the increasing button and I got "??" icon when decreasing the variable. How can I solve this issue ?Any help is appreciated.

This topic has been closed for replies.
Öyild.1
Öyild.1Best answer
Associate II
August 19, 2021

Hi,

I added 0-9 digits to not only default typography but also all typographies and it solved the problem. Thanks for helping.

4 replies

Alexandre RENOUX
Visitor II
August 19, 2021

Hello Öyild.1,

Here is an extract of the tutorial you're mentioning :

We need one more thing before the application is finished. TouchGFX only includes the characters needed, so we need to tell TouchGFX Designer to include the characters 0-9 in the "Default" typography. To do that, go back to TouchGFX Designer and click the "Texts" tab, then the "Typographies" tab. In the "Wildcard Ranges" column for the Default typography, add the range "0-9" (1).

As it explains, you need to add a Wildcard Range for TouchGFX to understand that it has to include all the digits from 0 to 9 when it compiles. Otherwise TouchGFX does not understand the character and replaces it by "?" instead.

/Alexandre

Öyild.1
Öyild.1Author
Associate II
August 19, 2021

Hi Alexandra RENOUX,

I have done already what you said but nothing changed. It is recommended to set wildcard range in tutorial so I did it. What kind of thing might cause such a problem?

Öyild.1
Öyild.1AuthorBest answer
Associate II
August 19, 2021

Hi,

I added 0-9 digits to not only default typography but also all typographies and it solved the problem. Thanks for helping.

Alexandre RENOUX
Visitor II
August 20, 2021

Hello Öyild.1,

Glad to hear your issue was fixed ^^

Please close this topic by choosing Select as Best.

/Alexandre