Skip to main content
Associate III
Oct 21, 2024 7:26 AM UTC
Question

display update frequency

Hi,

I am learning TouchGFX and I have gone through all the study materila from the TOuchGFX academy.

I am having a BW monochrome display on the SPI channel. And the display need not have to get updated unless there is a change in frame as the display itself has inbuilt RAM to store the framebuffer content. 

The question I have is, where the TouchGFX setting is to update the display in such case only when the framebuffer is change rather than updating the diplay on every tick (FPS)?

This topic has been closed for replies.

3 replies

ST Employee
Oct 21, 2024 3:00 PM UTC

Hello @mdalal,

For SPI displays, the procedure of handling the communication between TouchGFX and display is a bit different than LTDC. Please follow the documentations below to get an overview on how SPI displays are handled:

SPI Display Configuration 

TouchGFX Generator Display 

SPI and FMC Display Interface 

I hope this helps you!
If you have more questions, don't hesitate to ask!

Mohammad MORADIST Software Developer | TouchGFX
Tesla DeLorean
Guru
Oct 21, 2024 4:28 PM UTC

Failing an alert, CRC the frame buffer, to determine changes without holding a secondary copy.

You could also do regions of the frame too. If you have space you can keep a host side copy, and determine how many lines are impacted, or reduce to a region.

Some OS do track the scope/dimension of the changes to the frame buffer.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
mdalalAuthor
Associate III
Oct 22, 2024 4:54 AM UTC

Hi,

Thanks for the references. However, I still do not get a clear idea on how to set the frequency of the update.