Skip to main content
Okeskin
Associate III
Jan 22, 2026 9:36 AM UTC
Solved

Display the camera image using TouchGFX.

Hi ,

I'm developing a product on an STM32N6 using TouchGFX. I need to display the image coming from the camera input on the product on the TouchGFX. During our tests, we were able to directly print the image from the DCMI input to the screen and it worked. However, we need an example that takes this image and displays it on the TouchGFX. The AI ​​example prepared for the N6 actually includes this type of work, but the code is not accessible. Could you please share the relevant project or the relevant part so I can integrate it into my project, or could you provide an example project for this?

Osman SOYKURT
Osman SOYKURTBest answer
ST Technical Moderator
Aug 26, 2026 9:50 AM UTC

Hello,

An official example is now available in TouchGFX Designer (4.26.0) under Demos > Board Specific Demo:

 

 

ST Software Developer | TouchGFX

6 replies

Andrew Neil
Super User
Jan 22, 2026 10:08 AM UTC

@Okeskin wrote:

I need to display the image coming from the camera input on the product 


What camera?

What product?

How to write your question to maximize your chances to find a solution

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Okeskin
OkeskinAuthor
Associate III
Jan 22, 2026 10:42 AM UTC

I asked a very clear, general question.

I'm developing an HMI using the STM32N655. I'm using a PAL analog camera connected to the DCMI interface with this MCU. In our work, we displayed the camera image coming from DCMI directly on our screen via the LTDC interface using DMA. This was a test for hardware validation.

Currently, I'm working on displaying the live camera image from DCMI on the HMI I'm developing. Therefore, I need an example that displays the image from the DCMI interface using a widget on TouchGFX for the STM32N655.

I also have an STM32N6-DK. This demo kit includes a camera. In the demo software, the image from the camera is displayed to the user on the screen. If possible, I would prefer to share this example.

 

Okeskin_0-1769078558685.png

https://www.youtube.com/watch?v=aZTJaHHOA-4

 

 

Osman SOYKURT
ST Technical Moderator
Jan 26, 2026 1:34 PM UTC

Hello @Okeskin ,

We have made internally a project that runs on STM32N6 with the camera module shipped with the kit, which shows the camera stream in a TouchGFX application. Our intention is to make this available to everyone in TouchGFX Designer as a Board specific Demo (BSD). However, this demo is not yet finalized. I'll check with my team if we can still share the project in its current state before we'll make an official release of this demo. I'll write in this post again soon.

ST Software Developer | TouchGFX
Explorer II
Feb 23, 2026 8:56 PM UTC

Hello,

I'm also interested in this. Do you have an update about this you can share?

Osman SOYKURT
ST Technical Moderator
Feb 24, 2026 2:08 PM UTC
Osman SOYKURT
Osman SOYKURTBest answer
ST Technical Moderator
Aug 26, 2026 9:50 AM UTC

Hello,

An official example is now available in TouchGFX Designer (4.26.0) under Demos > Board Specific Demo:

 

 

ST Software Developer | TouchGFX