Skip to main content
JJ.Lin
Associate III
Jun 19, 2021 2:28 PM UTC
Question

Display doesn`t show after soft reset

Hi!,

My touchGFX application show nothing but the backlight is on as is expected after soft reset?Does anyone know the problem?

Thank you

This topic has been closed for replies.

3 replies

Romain DIELEMAN
ST Employee
Jun 21, 2021 6:38 AM UTC

Hi,

Are you working with a custom board or with a ST development kit ? Did you use an application template available in TouchGFX Designer ? Or use one as source of inspiration to configure your project ? Are you using an OS ? How did you configure your display (and what kind of display is it ? ) ?

/Romain

JJ.Lin
JJ.LinAuthor
Associate III
Jun 21, 2021 11:12 AM UTC

Hi,

I am working with a custom board, the CubeIDE is the latest version which generate the code of touchgfx and freertos. After upgrade, HAL_NVIC_SystemReset() is called , and it jump to the App code from boot, the screen show nothing but the backlight is normal as is expected.But after I put the power back on, the application work well.Do I need to deinit the LTDC or DMA2D peripheral before jump to app?

/Wayne

Associate II
Sep 19, 2023 10:33 AM UTC

Hi @JJ.Lin and @Romain DIELEMAN 

I have a similar problem like this. Is there any must to do while jumping from boot to the app?

How can I stop working TouchGFX?

Thanks in advance!

/Burak