Skip to main content
HTD
Senior II
Dec 8, 2023 8:11 PM UTC
Question

Designer: Importing and exporting custom containers - conflict resolving is missing.

I recently tried to use importing and exporting feature on custom container.

It works.

However, I encountered some very annoying problems:

Some of my custom container share resources, and sometimes I just need to create a couple of variations of the same custom container, like different theme.

By default, the generated manifest includes all affected parts. So - if I create several exports with the shared parts, then I include only my individual part - it works. However - it's quite tedious to maintain.

I have to export several files for 1 custom container, and remember to import them in the right sequence or it breaks.

The main problem is - when there's any resource conflict - the import just fails. There's no option to resolve the conflicts. The option to either leave existing resource or overwrite existing resource would totally fix it. I could export any number of versions of the same control and then decide what resources to import from it.

In the window area where yellow exclamation mark appears (conflict detected) - there should be a checkbox to overwrite the file. Unchecked - the existing file remains unchanged, if checked - existing file gets overwritten.

I guess it still can be done if I manually edited the manifest in the exported file (it's just a zip file). But this is basically creating another export files, that can be done by editing the manifest file on exporting. Doable but very tedious.

TL; DR - the options to resolve conflicts on custom container import is a very important feature that is missing in TouchGFX. This problem could be solved by just adding checkboxes indicating that the specified resources will be overwritten.

This topic has been closed for replies.

1 reply

Yoann KLEIN
ST Employee
Dec 11, 2023 8:52 AM UTC

Hello @HTD,

 

Thanks for your message. We are aware of this issue, and will improve the way CustomContainers import/export handles resources in a future release. I can't promise you a deadline for that though, it will depend on our other priorities.

 

Best regards.

Yoann KLEINST Software Developer | TouchGFX