Question
Demo firmware on STM32F769I-DISCO (not DISC1) with B-LCDAD-HDMI1
I have a STM32F769I-DISCO (Discovery board with LCD board) with the OEM firmware unchanged. I removed the LCD board and plugged in my B-LCDAD-HDMI1 (MB1232) board.
What should I expect to see on a monitor?
I've tried three different ones and it seems there's no signal out of the B-LCDAD-HDMI1.
If this is as expected, then what pre-built HEX file should I put on the DISC0 board so that I can test if my B-LCDAD-HDMI1 is defective or not?
Or is there some hardware difference between the DISCO (DISC0) and DISC1 variants that must be corrected first, (explained where, please)?
-Gary