Skip to main content
Pirol
Associate III
Sep 2, 2022 7:26 AM UTC
Question

Deleted Screens are not completely deleted

When I delete a Screen in TouchGFX Designer, the screen is deleted in the designer and the base files are also deleted. But the view and presenter files are not deleted. When I delete my user code in view and presenter, then these files are indeed deleted.

Why are the view and presenter files not deleted as long as there is user code inside?

I'm using TouchGFX Designer 4.20 with Keil.

The problem is the same as

https://community.st.com/s/question/0D53W00001gUvUbSAK/an-error-occurs-about-the-screen-deleted-from-touchgfx

but there is no good solution.

This topic has been closed for replies.

6 replies

Osman SOYKURT
ST Technical Moderator
Sep 6, 2022 9:11 AM UTC

Hello Pirol,

Yes you're right, when you create screens and then you delete them, some files (user code files) still remains. This is not a bug but made on purpose to don't erase accidentally any code that you might need to copy/move to another file. Indeed, the "generate code" purpose isn't to clean code, especially those written by the user. So if you delete screens, you'll need to do it manually.

/Osman

ST Software Developer | TouchGFX
Pirol
PirolAuthor
Associate III
Sep 6, 2022 12:08 PM UTC

Hello Osman,

thanks for your answer.

Ok, I can delete the files by hand.

But why is it not enough to exclude the files from the Keil project? I would expect: when neither the files of a screen (view+presenter) are included in the uvprojx nor the screen is existent in the TouchGFX Designer, than the files should be ignored by the code generator of TouchGFX Designer. But they are not. A screen deleted in Designer and excluded from Keil pops up in Keil everytime I generate the code from the designer. Is that also on purpose?

Osman SOYKURT
ST Technical Moderator
Sep 6, 2022 1:18 PM UTC

Hi again,

I've just made the test on my side, and deleted screens files are not included in my Keil project. So I can't reproduce your issue. Which version of Keil are you using ? I'm working with uVision V5.32.0.0, and it works perfectly fine here. Do you have this kind of popup on Keil whenever you regenerate code on TouchGFX Designer ?

0693W00000SucD2QAJ.png 

/Osman

ST Software Developer | TouchGFX
Pirol
PirolAuthor
Associate III
Sep 6, 2022 1:57 PM UTC

Hello Osman,

I'm using Keil 5.29.0.0.

The pop up shows up most of the times, sometimes not. But the new code is there even without the pop up.

If I do the following steps, I get the strange behaviour. The project consists of four screens with very few widgets on them. There is some user code in screen4.

- Delete screen4 in the Designer and generate code.

- Remove screen4.cpp from Keil.

- Create a custom container in the Designer and add it to a screen; regenerate.

--> In Keil, both the container and Screen4 show up in the project tree.

- Remove Screen4 again and add some code to the custom container.

- Delete the custom container in the Designer (completely, not only on the screen); regenerate.

--> Screen4 shows up again and CustomContainer1 is still there.

Just to be clear: The files of screen4 are not recreated (I haven't deleted them in the previous steps). It's just the path in Keil that is recreated. When I delete the files of screen4, they do not show up again. So it's not a big problem, because I could just delete the files, but I found it quite strange.

Osman SOYKURT
ST Technical Moderator
Sep 13, 2022 8:00 AM UTC

Hey Pirol,

I tried the steps you wrote, I don't have the same behavior. When I delete the screen4 in designer, the screen4View.cpp and screen4Presenter.cpp will automatically be deleted from my Keil project tree (purpose of the popup asking for project reload). And if I add more widgets on my others screens, the sceen4 doesn't show up.

I don't have other idea than updating your Keil to version V5.32.0.0. Can you try with that ?

/Osman

ST Software Developer | TouchGFX