Skip to main content
mArSat
Associate II
Feb 6, 2025 10:57 AM UTC
Solved

Debug Issue with STM32H7B3I-DK and TouchGFX 4.24.2 in STM32CubeIDE 1.17.0


Issue Description


I am experiencing a debugging issue with a project generated using TouchGFX Designer 4.24.2 for STM32H7B3I-DK, running on STM32CubeIDE 1.17.0. When I attempt to start debugging, I get the following error:

 

 

 

Failed to execute MI command:
load C:\TouchGFXProjects\Test01\STM32CubeIDE\Debug\STM32CubeIDE.elf
Error message from debugger back end: Load failed

 

 

 

Tests Performed

  1. Project generated with TouchGFX 4.24: If I generate the project from TouchGFX and try to debug, I get the error mentioned above.
    The firmware loads correctly when flashed (.hex) manually via STM32CubeProgrammer, but the graphics appear corrupted.
  2. Empty STM32CubeIDE Project (No TouchGFX): If I create a new empty project for the STM32H7B3I-DK in STM32CubeIDE 1.17.0, the debugger works without any issues.


Flashing and debugging function properly.

Observations

  1. The issue seems specific to projects generated using TouchGFX 4.24.2
  2. There might be a problem with memory configuration, linker scripts, or how TouchGFX handles the flash.

Questions

  • Has anyone experienced a similar issue with TouchGFX projects?
  • Are there specific settings required in STM32CubeIDE to properly debug a TouchGFX project on STM32H7B3I-DK?
  • Could this be related to flash memory configuration in linker scripts?

 

Any help or suggestions would be greatly appreciated.

This topic has been closed for replies.
mArSat
mArSatBest answer
Associate II
Feb 6, 2025 3:18 PM UTC

# Issue Resolved: Debugging & Graphical Corruption in TouchGFX with STM32H7B3I-DK

I encountered an issue when debugging a TouchGFX project for the **STM32H7B3I-DK** using **STM32CubeIDE 1.17.0** and **TouchGFX Designer 4.24.2**. Initially, when launching the project from **TouchGFX Designer**, the debugger failed to load the `.elf` file, and when flashing the `.hex`, the application would run, but the **graphics were corrupted**.

---

## Solution

### 1. Modify the Linker File (`STM32H7B3LIHXQ_FLASH.ld`)
- I changed the memory sections for:
- `FontFlashSection`
- `TextFlashSection`

- These were originally set to `OSPI`, and I changed them to `FLASH`.
- This ensures that assets are stored in the **internal flash** instead of external **OSPI** memory.

### 2. Update TouchGFX Designer Settings
- Previously, in **Default Image Configuration**, the **Section** and **Extra Section** were set to `ExtFlashSection`.
- I changed both to `IntFlashSection`.

---

## Results
- Debugging now works properly in STM32CubeIDE.
- The graphical corruption issue is completely resolved.
- The application runs as expected on the STM32H7B3I-DK.

---

## Recommendations
If anyone else encounters similar issues, I recommend:
- Checking the **memory mappings** in the linker script.
- Ensuring **TouchGFX assets** are stored in the correct flash memory.

Hope this helps!

1 reply

mArSat
mArSatAuthorBest answer
Associate II
Feb 6, 2025 3:18 PM UTC

# Issue Resolved: Debugging & Graphical Corruption in TouchGFX with STM32H7B3I-DK

I encountered an issue when debugging a TouchGFX project for the **STM32H7B3I-DK** using **STM32CubeIDE 1.17.0** and **TouchGFX Designer 4.24.2**. Initially, when launching the project from **TouchGFX Designer**, the debugger failed to load the `.elf` file, and when flashing the `.hex`, the application would run, but the **graphics were corrupted**.

---

## Solution

### 1. Modify the Linker File (`STM32H7B3LIHXQ_FLASH.ld`)
- I changed the memory sections for:
- `FontFlashSection`
- `TextFlashSection`

- These were originally set to `OSPI`, and I changed them to `FLASH`.
- This ensures that assets are stored in the **internal flash** instead of external **OSPI** memory.

### 2. Update TouchGFX Designer Settings
- Previously, in **Default Image Configuration**, the **Section** and **Extra Section** were set to `ExtFlashSection`.
- I changed both to `IntFlashSection`.

---

## Results
- Debugging now works properly in STM32CubeIDE.
- The graphical corruption issue is completely resolved.
- The application runs as expected on the STM32H7B3I-DK.

---

## Recommendations
If anyone else encounters similar issues, I recommend:
- Checking the **memory mappings** in the linker script.
- Ensuring **TouchGFX assets** are stored in the correct flash memory.

Hope this helps!