Skip to main content
Hben.1
Associate
June 14, 2021
Question

Debug Error with Touchgfx

Hi.

board : stm32L4R9-EVAL

LCD : MB1315A

TouchGFX version : 4.16.1

STM32CubeMX : 6.2.1

​

I try to get index of scrollList selected.

before add callback function, debugging is work.

However If I add callback function, Debugging is Strange.

(Some function is removed. I don't want to show.)

In View. hpp

class SearchScreenView : public SearchScreenViewBase
{
public:
 SearchScreenView();
 virtual ~SearchScreenView() {}
 virtual void setupScreen();
 virtual void tearDownScreen();
 
protected:
	Callback<SearchScreenView, int16_t> scrollListItemSelectedCallback;
	void scrollListItemSelectedHandler(int16_t itemSelected);
 
};

in view.cpp

SearchScreenView::SearchScreenView() : scrollListItemSelectedCallback(this, &SearchScreenView::scrollListItemSelectedHandler)
{
 
}
 
void SearchScreenView::setupScreen()
{
 SearchScreenViewBase::setupScreen();
 ScrollList.setItemSelectedCallback(scrollListItemSelectedCallback);
 
 
}
 
void SearchScreenView::tearDownScreen()
{
 SearchScreenViewBase::tearDownScreen();
}
 
void SearchScreenView::scrollListItemSelectedHandler(int16_t itemSelected)
{
	printf("Selected Index : %d\n",itemSelected);
}

If I start to debug

​

in main.c

/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();
 
 /* USER CODE BEGIN Init */
 
 /* USER CODE END Init */
 
 /* Configure the system clock */
 SystemClock_Config();
 
 /* USER CODE BEGIN SysInit */
 
 /* USER CODE END SysInit */
 
 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_DMA_Init();
 MX_CRC_Init();
 MX_DMA2D_Init();
 MX_I2C2_Init();
 MX_LTDC_Init();
 MX_UART4_Init();
 MX_TouchGFX_Init();
 /* USER CODE BEGIN 2 */
 
 printf("START\n");

in main.c after line 23, debugging happened error.

can not excute next line.

debug arrow is disappeared, I try to suspend.

and then address is moved strange address. like under screenshot.

​0693W00000BarY7QAJ.jpg​

​If I remove callback function, it is work normally.

another strange is If I run , not debug mode, it is work well.

the program is run well except can not debug.

Could you give any advice?

thank you.

This topic has been closed for replies.

2 replies

MM..1
Super User
June 14, 2021

Try remove printf from handler

Hben.1
Hben.1Author
Associate
June 15, 2021

thank you relpy

but it is not work.