Skip to main content
CHou.1
Associate II
July 12, 2021
Question

DCMI Frame event when receiving JPEG image

Hoping for some guidance on DCMI implementation when receiving JPEG images. I am currently successfully receiving JPEG data over the DCMI interface using snapshot mode.The main issue is that the DCMI_FrameEventCallback does not seem to trigger so I am currently just waiting a couple of seconds before reading the buffer (the Vsync and Line callbacks are working though).

As far as I can tell, the DCMI_FrameEventCallback is a DCMI concept which would only be triggered once the specified length passed to the DCMI_Start_*** function is met. This is kinda hard to do when working with JPEG images.

Just wondering if anyone had to deal with this issue before. Thanks!

This topic has been closed for replies.