Skip to main content
ktrofimo
Senior III
January 30, 2022
Question

D-Cache failed again?

While heavy updating customized DynamicGraph after some time (from 10 minutes to more then an hour) application goes to HardFault.

Investigation shows that problem always happens inside TouchGFX library function CWRUtil::Q5 indexToScreenXQ5( const AbstractDataGraph *graph, const int16_t index const );

Failing code:

ldr r3, [r1, #0]

mov r0, r1

mov r1, r2

ldr.w r3, [r3, #212] <-- HardFault

bx r3

registers at time of HardFault:

r0 = 0x2400f124

r1 = 0x00000130

r2 = 0x00000130

r3 = 0x001c0002 <-- problem! usually it equals to 0x080924ac

So it should go this way:

r3 = &(0x2400f124) = 0x080924ac

0x080924ac + 212 = 0x8092580

&(0x8092580) = 0x0806865d

jump to 0x0806865d (indexToScreenXQ5)

But when it fails:

r3 = &(0x2400f124) = 0x001c0002

0x001c0002 + 212 = 0x001c00d6

&(0x001c00d6) = xxxx

HardFault

P.S.

0x2400f124 - correct pointer to graph class in SRAM

0x080924ac - correct graph class flash code location

0x001c0002 - incorrect (invalid address)

This topic has been closed for replies.

3 replies

ktrofimo
ktrofimoAuthor
Senior III
January 30, 2022

Yes. It is D-Cache not updating properly problem.

Call to ​SCB_CleanInvalidateDCache(); before copying quite large amount of data helps.

Uptime 9h for now and no HardFaults

Romain DIELEMAN
ST Employee
January 31, 2022

What MCU are you using again ? What version of TouchGFX did you try it with ?

/Romain

ktrofimo
ktrofimoAuthor
Senior III
January 31, 2022

MCU: STM32H743IIT6

STM32CubeIDE Version: 1.7.0

ARM CMSIS 5.7.0

Cube IDE STM32H7 MCU package 1.9.1

TouchGFX 4.17.0

​

"Again" - because I ​already had similar issues with D-Cache: https://community.st.com/s/question/0D53W00001K3F7WSAV/why-dcache-invalidation-hangs