Skip to main content
ivanbraga
Associate
Mar 23, 2019 4:37 AM UTC
Question

Custom plate, is there a way to implement it in CubeMX? Or did I miss something?

I'm working on a custom board, where I'm introducing new features and testing each individually.

Example:

LTDC with the cubemx interface. Tested the operation. OK.

FMC with the cubemx interface. Tested the operation. OK.

DMA2D with the cubemx interface. Tested the operation. OK.

In short, I have to create each configuration separately, and the worst individually for each pin, because many pins appear set by default in CubeMX.

And there is a detail that I do not understand!

Why can not I copy all libraries when I'm in TrueSTUDIO, but when in MKD can I?

Since TrueSTUDIO is from ST, can not I manually configure my projects?

As I have an Eastern origin, I will patiently wait for software developers, contractors and CubeMX managers, "to graduate in the Faculty of Software Engineering, to explain this lesson I lost, I apologize for being an absent and inattentive student. "

Ivan Braga

This topic has been closed for replies.