Skip to main content
ANapa
Associate III
February 7, 2022
Solved

Custom bootloader. MCU STM32H7BIT Application use FreeRTOS and TouchGfx. Some issues.

Hi,

I build a custom bootloader.

Trying to load app on FreeRTOS and TouchGfx

MCU - STM32H7BIT

The MCU has 2 FLASH banks:

0x08000000 - 1024k

0x08100000 - 1024k

gcc-arm-none-eabi toolchain.

openocd for loading and debuging.

The app works fine when loaded at 0x08000000. FLASH origin.

Next...

Begin Option 1:

-------------------------------------------------- --------------------------------------------------

The application works after loading from the bootloader if stored at 0x08100000.

I do in bootloader:

void Bootloader_JumpToApplication (void)

{

     HAL_RCC_DeInit();

     HAL_DeInit();

     /* Disable SysTick */

     SysTick->CTRL = 0;

     SysTick->LOAD = 0;

     SysTick->VAL = 0;

     __asm("B 0x0812E700"); // Address obtained from *.map file

                // This is the address of Reset_Handler

}

In the application *.ld file

FLASH(rx): ORIGIN=0x08100000, LENGTH=2048K

SCB->VTOR = 0x08100000; By some miracle. Without my participation.

However I do:

SCB->VTOR = 0x08100000; At the very beginning of main(), in the application, just in case.

-------------------------------------------------- --------------------------------------------------

End Option 1:

Begin Option 2:

-------------------------------------------------- --------------------------------------------------

Does not work!

Application downloaded at 0x08060000

In the application *.ld file

FLASH(rx): ORIGIN=0x08060000, LENGTH=2048K

In the bootloader:

void Bootloader_JumpToApplication (void)

{

     HAL_RCC_DeInit();

     HAL_DeInit();

     /* Disable SysTick */

     SysTick->CTRL = 0;

     SysTick->LOAD = 0;

     SysTick->VAL = 0;

     __asm("B 0x0808E890"); // Address obtained from *.map file

                 // This is the address of Reset_Handler

}

SCB->VTOR = 0x08060000; At the very beginning of main(), in the application.

QtCreator memory viewer shows that this measurement value in the SCB->VTOR area is correct.

Application continues to run...

After that, a Hard Fault occurs.

Undefined instruction (UNDEFINSTR)

Invalid function call address 0x58024400 - Very strange address!

XPSR 0x41000003

PC 0x80014FA - Very strange address!

SP 0x2001FFBC

-------------------------------------------------- ----------------------------------

End Option 2:

Begin Option 3:

-------------------------------------------------------------------------------------

If exclude the TouchGfx task from the application, then everything works with any place of the applications.

At the same time, FreeRTOS works:

osThreadDef(touchTask, taskTouch, osPriorityNormal, 0, 128);

touchTaskHandle = osThreadCreate(osThread(touchTask), NULL); // Tracks i2c touchscreen events

osThreadDef(logTask, taskLog, osPriorityNormal, 0, 128);   // Send debug strings to UART6

logTaskHandle = osThreadCreate(osThread(logTask), NULL);

I can rewrite all SDRAM by touching the touchscreen.

Screen fill colors change as I conceived and programmed.

UART6 prints my debug lines

-------------------------------------------------------------------------------------

End Option 3:

The problem is in TouchGfx???

This topic has been closed for replies.
ANapa
ANapaBest answer
Associate III
February 7, 2022

It seems that the problem was solved by careful selection of smaller stack sizes for FreeRTOS tasks.

Downloads of various applications with a custom loader now work.

1 reply

ANapa
ANapaAuthorBest answer
Associate III
February 7, 2022

It seems that the problem was solved by careful selection of smaller stack sizes for FreeRTOS tasks.

Downloads of various applications with a custom loader now work.