Skip to main content
ADu P.1
Visitor II
Feb 23, 2020 12:35 PM UTC
Question

Custom board with 5" and 7" TFT display Tutorial

Is there any tutorials on creating a custom board with a cheap 5" or 7" TFT Touch screen? The only cheap disco board STM32f746G Disco only has a 4.3" screen. I need something bigger unfortunately.

I assume a lot of other components would also be required for the basics, ex RAM/ROM/Flash etc. Total newbie here though :)

This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
Feb 23, 2020 2:30 PM UTC

The displays usually have Datasheets describing the expectations and parameter ranges for driving the panel.

​

The resolution drives the memory size, pixel clock and bandwidth.

​

Decide if you want a display with a controller, parallel interface, or DSI.​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..