Skip to main content
JBlac
Associate III
Dec 7, 2018 4:00 PM UTC
Question

cubemx fmc setup for stemwin and STM32F767ZI

​I'm trying to use cubemx to setup a project to use STEMWIN on my nucleo 144 board; however, I'm having a problem with FMC setup, specifically, I get a yellow triangle on SDRAM1 and SDRAM2.  I'm not exactly sure how to configure these for use with the HX8357C LCD display.  I was looking in the datasheet for the display and it mentions is has 2 banks of ram, so that's what I specified in both SDRAMx sections, but I can't seem to get rid of the yellow warning triangles as it says I have a conflict, but what it is I don't know.  Perhaps there's an example that I could build upon?

Thanks.

This topic has been closed for replies.

2 replies

Vitaliy Chernobay
Senior
Dec 9, 2018 8:39 AM UTC

HX8357C  is not RGB display!

JBlac
JBlacAuthor
Associate III
Dec 9, 2018 1:00 PM UTC

Hmmmm, where did you come up with that response? Do a search for HX8357 datasheet and you will find that it is, indeed, a RGB 480 x 320 TFT LCD display! It is, in fact, very much like the ILI9481 display. Nevertheless, I was looking for information about configuring the SDRAM1/2 sections in CubeMx. Your answer is of no help, so why respond?