Solved
CubeMX does not allow use of THREADX with TouchGFX on TrustZone-enabled U5 project
- 3 replies
- 1960 views
Hi,
For TrustZone enabled project (U5), TouchGFX configuration in CubeMX can't recognize enabled THREADX.
Any ideas?
Two screenshots attached:
one for TrustZone enabled project setup and another one for the exact same but Non-TrustZone project.
For the former it can be seen that THREADX option is greyed-out and cannot be selected, while for latter everything highlighted as expected.
CubeMX generates correct project for non-TrustZone enabled project.
TouchGFX version is 23.1, CubeMX is 6.10.0
Thanks