Skip to main content
MEder
Associate III
Feb 20, 2019 3:50 PM UTC
Question

CubeMX, Atollic, TouchGFX framework Directory

I have a STM32F746G-Discovery board and the CubeMX and TouchGFX project setup in Atollic.

Much of it is functioning. However when I went to edit in the TouchGFX​ Designer, I had compilation errors when generating code.

It seems the Directory  \STM32F746DiscoTemplate\STM32F746-DISCO\TouchGFX\touchgfx  is missing.

it is now in \Middlewares\ST

Now I have redundant copies on disk,  is there a solution?

Thanks

This topic has been closed for replies.

4 replies

MEder
MEderAuthor
Associate III
Feb 20, 2019 4:59 PM UTC

​Here's the Output_CompileSimulator.log

Converting images

Compiling simulator/main.cpp

Compiling ../Middlewares/ST/TouchGFX/touchgfx///framework/source/platform/driver/touch/SDL2TouchController.cpp

simulator/main.cpp:1:51: fatal error: platform/hal/simulator/sdl2/HALSDL2.hpp: No such file or directory

#include <platform/hal/simulator/sdl2/HALSDL2.hpp>

^

compilation terminated.

../Middlewares/ST/TouchGFX/touchgfx///framework/source/platform/driver/touch/SDL2TouchController.cpp:17:51: fatal error: platform/hal/simulator/sdl2/HALSDL2.hpp: No such file or directory

#include <platform/hal/simulator/sdl2/HALSDL2.hpp>

^

compilation terminated.

simulator/gcc/Makefile:220: recipe for target 'build/MINGW32_NT-6.2/simulator/main.o' failed

make[2]: *** [build/MINGW32_NT-6.2/simulator/main.o] Error 1

make[2]: *** Waiting for unfinished jobs....

simulator/gcc/Makefile:212: recipe for target 'build/MINGW32_NT-6.2/touchgfx/framework/source/platform/driver/touch/SDL2TouchController.o' failed

make[2]: *** [build/MINGW32_NT-6.2/touchgfx/framework/source/platform/driver/touch/SDL2TouchController.o] Error 1

simulator/gcc/Makefile:182: recipe for target 'generate_assets' failed

make[1]: *** [generate_assets] Error 2

simulator/gcc/Makefile:40: recipe for target 'all' failed

make: *** [all] Error 2

eng23
Senior
Feb 21, 2019 12:55 PM UTC

Hello,

I think you need to exclude from build the folder simulator like this step:

10)     Close project properties. In the ‘Project Explorer’, go through the folders and for all ‘template’ files and other IDE types, use a right click menu ‘Resource Configuration’->’Exclude from Build’ (select all configurations) to keep them from being compiled. The same for the whole folders ‘build’ and ‘simulator’ under folder ‘TouchGFX’.

MEder
MEderAuthor
Associate III
Feb 21, 2019 1:53 PM UTC

​I think your referring to Compiling the Project in Atollic or other IDE.  I am referring to the Generate Code Button in TouchGFX designer. 

The Error occurred one more time while I had the Designer open as well as the Atollic Project. ( and with the toughgfx directory copied ) It might just be a oddball problem when both are open.  The '///'  in the Error log looks like a improper path, for some reason it does not occur all the time.

FYI, It was the first time that I had edited the original ToughGFX project after creating it via CubeMX.

Thanks

eng23
Senior
Feb 21, 2019 2:08 PM UTC

Ok sorry, you are right!

I have the same problem in TouchGFX Designer, but if I click Generate Code it compiles ok. This problem occurs only when the TouchGFX is compiling by itself (it seems like it compiles all the time).