Senior
May 29, 2018 11:15 PM UTC
Solved
CubeMx 4.25 & STemWin & WM_MULTIBUF_Enable(1)
- 7 replies
- 1448 views
Posted on May 30, 2018 at 01:15
I make the small project for F746 Discovery with STemWin (small test window with button) for Keil
After the project is compiling & the start - black screen.
void GRAPHICS_Init(void)
{/* Initialize the GUI */GUI_Init();WM_MULTIBUF_Enable(1);
/* Enable the multi-buffering functionality *//* Activate the use of memory device feature */
/* USER CODE BEGIN WM_SetCreateFlags *///WM_SetCreateFlags(WM_CF_MEMDEV);/* USER CODE END WM_SetCreateFlags */}I am a comment line
//WM_MULTIBUF_Enable(1);
An image appears on the screen after this.
Why does not WM_MULTIBUF_Enable(1) work?
#stemwin #cubemx #multibuf