Skip to main content
Kss.1
Associate II
July 28, 2020
Solved

CubeIDE compile error ADC input LCD display

​

https://www.youtube.com/watch?v=EbWOv_0Lp-U&t=1873s

I watched YouTube and followed it. This is to display the voltage coming into ADC IN0 on the LCD.

I used the TouchGFX + CubeIDE compiler, but an error occurred.

On YouTube, it compiles normally. Please let me know why the error occurred.

​

make -j12 all 

arm-none-eabi-g++ "../TouchGFX/gui/src/screen1_screen/Screen1View.cpp" -mcpu=cortex-m7 -std=gnu++14 -g3 -DUSE_HAL_DRIVER -DSTM32F746xx -DDEBUG -c -I../TouchGFX/gui/include -I../TouchGFX/generated/fonts/include -I"C:/ST/STM32CubeIDE_1.3.0/SWTEST/Drivers/Components" -I"C:/ST/STM32CubeIDE_1.3.0/SWTEST/Drivers/Components/n25q128a" -I../TouchGFX/generated/texts/include -I../Drivers/STM32F7xx_HAL_Driver/Inc -I../TouchGFX/generated/images/include -I"C:/TouchGFXProjects/SWITCHTEST/Drivers/Components/Common" -I"C:/ST/STM32CubeIDE_1.3.0/SWTEST/Drivers/Components/ft5336" -I"C:/TouchGFXProjects/SWITCHTEST/Drivers/Components/n25q128a" -I../Core/Inc -I../TouchGFX/generated/gui_generated/include -I"C:/ST/STM32CubeIDE_1.3.0/SWTEST/Drivers/Components/Common" -I"C:/TouchGFXProjects/SWITCHTEST/Drivers/Components/ft5336" -I../Middlewares/Third_Party/FreeRTOS/Source/CMSIS_RTOS -I../Drivers/STM32F7xx_HAL_Driver/Inc/Legacy -I../Middlewares/Third_Party/FreeRTOS/Source/include -I../Drivers/CMSIS/Device/ST/STM32F7xx/Include -I../Middlewares/ST/touchgfx/framework/include -I"C:/ST/STM32CubeIDE_1.3.0/SWTEST/Drivers/BSP" -I../TouchGFX/target/generated -I../Drivers/CMSIS/Include -I../Middlewares/Third_Party/FreeRTOS/Source/portable/GCC/ARM_CM7/r0p1 -I../TouchGFX/App -I../TouchGFX/target -O0 -ffunction-sections -fdata-sections -fno-exceptions -fno-rtti -fno-threadsafe-statics -fno-use-cxa-atexit -Wall -fstack-usage -MMD -MP -MF"TouchGFX/gui/src/screen1_screen/Screen1View.d" -MT"TouchGFX/gui/src/screen1_screen/Screen1View.o" --specs=nano.specs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -o "TouchGFX/gui/src/screen1_screen/Screen1View.o"

../TouchGFX/gui/src/screen1_screen/Screen1View.cpp: In member function 'virtual void Screen1View::analogUpdate(uint32_t)':

../TouchGFX/gui/src/screen1_screen/Screen1View.cpp:19:10: error: 'textAreaADBuffer' was not declared in this scope

 memset(&textAreaADBuffer, 0, TEXTAREAAD_SIZE);

     ^~~~~~~~~~~~~~~~

../TouchGFX/gui/src/screen1_screen/Screen1View.cpp:19:10: note: suggested alternative: 'textArea1'

 memset(&textAreaADBuffer, 0, TEXTAREAAD_SIZE);

     ^~~~~~~~~~~~~~~~

     textArea1

../TouchGFX/gui/src/screen1_screen/Screen1View.cpp:19:31: error: 'TEXTAREAAD_SIZE' was not declared in this scope

 memset(&textAreaADBuffer, 0, TEXTAREAAD_SIZE);

                ^~~~~~~~~~~~~~~

../TouchGFX/gui/src/screen1_screen/Screen1View.cpp:19:31: note: suggested alternative: 'TEXTAREA_HPP'

 memset(&textAreaADBuffer, 0, TEXTAREAAD_SIZE);

                ^~~~~~~~~~~~~~~

                TEXTAREA_HPP

../TouchGFX/gui/src/screen1_screen/Screen1View.cpp:21:2: error: 'textAreaAD' was not declared in this scope

 textAreaAD.invalidate();

 ^~~~~~~~~~

../TouchGFX/gui/src/screen1_screen/Screen1View.cpp:21:2: note: suggested alternative: 'textArea1'

 textAreaAD.invalidate();

 ^~~~~~~~~~

 textArea1

make: *** [TouchGFX/gui/src/screen1_screen/subdir.mk:23: TouchGFX/gui/src/screen1_screen/Screen1View.o] Error 1

"make -j12 all" terminated with exit code 2. Build might be incomplete.

I saw your YouTube and tried it. However, some errors have occurred.

Some variables are not declared, how can I solve them?

void Screen1View::analogUpdate(uint32_t value)

{

memset(&textAreaADBuffer, 0, TEXTAREAAD_SIZE);

Unicode::snprintfFloat(textAreaADBuffer, sizeof(textAreaADBuffer), "%.3f", value * 0.000805664 ); // 3.3/4096 = 0.000805664

textAreaAD.invalidate();

}

I tried to display the analog input voltage on the LCD screen, but an error occurred in the screen viewer function. The problem made me sick for a week. I want to upload a proper YouTube. The person who uploaded YouTube wants to upload in detail how the error did not occur.

Can someone please help me.

It seems crazy.

This topic has been closed for replies.
prain
prainBest answer
Visitor II
July 30, 2020

In ADC conversion complete callback, set a flag. Use this flag to poll for end of conversion. ​then reinitialize ADC conversion.

12 replies

prain
Visitor II
July 28, 2020

your problem is related to scopes in c++ . search for textAreaADBuffer and ​TEXTAREAAD_SIZE. make sure these are defined or included in file Screen1View.cpp

Kss.1
Kss.1Author
Associate II
July 30, 2020

screen1View.hpp

I resolved it by declaring as below.

#ifndef SCREEN1VIEW_HPP

#define SCREEN1VIEW_HPP

#include <gui_generated/screen1_screen/Screen1ViewBase.hpp>

#include <gui/screen1_screen/Screen1Presenter.hpp>

class Screen1View : public Screen1ViewBase

{

public:

  Screen1View();

  virtual ~Screen1View() {}

  virtual void setupScreen();

  virtual void tearDownScreen();

  virtual void analogUpdate(uint32_t value);

protected:

  static const uint16_t TEXTVIEW_BUFF_SIZE = 50;

         Unicode::UnicodeChar textViewBuffer[TEXTVIEW_BUFF_SIZE];

};

#endif // SCREEN1VIEW_HPP

prain
Visitor II
July 30, 2020

Sounds like you are missing a directory from your include path.

Kss.1
Kss.1Author
Associate II
July 30, 2020

Compilation was successful. I downloaded it to the 746 board, but the LCD screen is broken. I chose LTDC as the RGB565 format 16bit, but I can't tell.

Why is the screen broken?

prain
Visitor II
July 30, 2020

There are LCD examples for your board​. Did you try them?