Skip to main content
FJB2069
Senior
Feb 14, 2025 9:00 PM UTC
Question

Create/Copy new TouchGFX/CubeIDE project with different package

I would like to take my existing stm32F746G-DISCO CubeIDE project, copy it and only change the chip from the STM32F746NGHx  218 BGA to the STM32F746IGTx 176 LQFP

I can copy the project, but I don't see a way to change the chip.  In the .IOC file under Pinouts you can search for pin compatible MCU's, but won't bring up 176 LQFP.    Obviously not pin compatible.

I have already re-worked the Altium schematics to use the 176 LQFP chip.  My project eliminates several peripherals and changes some of the pins, but I figured can re-assign them in the new .IOC file?

I am assuming I will need to create a new MXCUBE or TouchGFX project for the correct chip and then copy from working project to new project?

Any insight appreciated!

 

 

 

 

 

This topic has been closed for replies.

2 replies

STTwo-32
ST Technical Moderator
Feb 14, 2025 9:40 PM UTC

Hello @FJB2069 

On a .IOC file, you can’t change the MCU and keep the configurations. So, as you said, you should create a new project and migrate you configuration on it.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
ST Employee
Feb 17, 2025 9:42 AM UTC

Hello @FJB2069 ,

If you have a Tgfx project for your chip, you can import the UI from another one by clicking on Edit/Import/Gui.

LouisB_0-1739785297880.png

BR,

Louis BOUDOST Software Engineer | TouchGFX