Skip to main content
ihsanoglu
Senior
Mar 5, 2019 7:07 AM UTC
Question

Configuring project for Keil rather than EWARM

Hello everybody

I am trying to configure a project for STM32F746-DISCO board with TouchGFX using CubeMx. A new project.

However , the article for configuring the board at this link explains the modifications needed for linker script and modifying the project for EWARM only, as far as I understand

I am using Keil , how can I modify the linker script in the same manner ?

I hope I didn't miss anything

This topic has been closed for replies.

5 replies

Martin KJELDSEN
Principal III
Mar 6, 2019 12:38 PM UTC

Hi @Abdullah İhsanoğlu​,

Some background info. Version 2.0.0 of the F7 based Application Templates in TouchGFX have been updated with the fixes in the articles that you refer to. But only for EWARM and gcc. There's no guide for how to do this for Keil yet, but the goal is that CubeMX should just produce working projects and until it does the ATs in TouchGFX will do that work for you - So, yeah, i apologize, but we're not quite there yet adding CubeMX + all compiler support for all ATs.

But it's a big red flag here because people are having such difficulty getting started with CubeMX+TouchGFX.

I promise i'll keep you updated once we progress on the issue.

If you send me your project, maybe i can take a look.

Best regards,

Martin

ihsanoglu
ihsanogluAuthor
Senior
Mar 6, 2019 12:48 PM UTC

Well , first thank you for your reply I really appreciate it

So if I used gcc with eclipse ( Although I don't prefer to ) I will be able to compile the projects without any problems? If I understand this clearly I hope you breifly mention how to create such a template as the articles explaining for IAR only.

now , I would like to send you a project , but there isn't one. In fact I am trying to start an empty project to start development since I want to migrate from another framework to TouchGfx.

I appreciate any help you can provide.

Thank you,

İhsanoğlu