Configuration of STM32H750B-DK with TouchGFX
- 2 replies
- 414 views
I'm trying to configure the LCD display using STM32CubeMX for the STM32H750B-DK.
Under the Middleware and Software Packs, in X-CUBE-TOUCHGFX, under the TouchGFX Generator tab, I get a Dependency Error in red:
Width/height values must equal LTDC Window width/height.
I think I've selected the values properly to do that: 480 x 272 (right?), and adjusted for the other places these values go. The result of this error is the code generation emits the expected warning, and BlitOp.h/.cpp isn't produced, causing the build to fail.
I've attached my ioc file as a zip file.
I am stuck on this and don't see what to adjust. I am essentially trying to get a "Hello World" application to run, although I haven't actually modified anything except the Makefile so far (also attached).
If I deselect TouchGFX, there are no warnings from the code generation step and the build completes.
Thanks!
Chris