Skip to main content
DMacD.1
Associate II
Mar 24, 2022 9:04 PM UTC
Question

Compiling to Target issue with Callbacks

Code works fine in simulator but compilation to target (STM32756G-eval2).

Code:

// MainDisplayView.cpp
 
MainDisplayView::MainDisplayView(): 
 viewCallback(this, &MainDisplayView::buttonNavCallbackHandler),
 boxClickedCallback1(this, &MainDisplayView::boxClickedHandler1),
 boxClickedCallback2(this, &MainDisplayView::boxClickedHandler2)
{
 buttonLeft.setViewCallback(viewCallback);
 buttonRight.setViewCallback(viewCallback);
 overtempSetting1.setClickAction(boxClickedCallback1);
 durationSetting1.setClickAction(boxClickedCallback2);
}

Error:

 TouchGFX/gui/src/maindisplay_screen/MainDisplayView.cpp: In constructor 
 'MainDisplayView::MainDisplayView()':
 
TouchGFX/gui/src/maindisplay_screen/MainDisplayView.cpp:10:71: error: invalid use of non-static member function 'void MainDisplayView::buttonNavCallbackHandler(const buttonImportant&)'
 boxClickedCallback2(this, &MainDisplayView::boxClickedHandler2)
 ^ 
In file included from TouchGFX/gui/src/maindisplay_screen/MainDisplayView.cpp:1:0: TouchGFX/gui/include/gui/maindisplay_screen/MainDisplayView.hpp:60:10: note: declared here void 
 buttonNavCallbackHandler(const buttonImportant &b);
 ^~~~~~~~~~~~~~~~~~~~~~~~
 gcc/Makefile:320: recipe for target 'TouchGFX/build/STM32756G-EVAL/TouchGFX/gui/src/maindisplay_screen/MainDisplayView.o' failed
 

Particularly the error "invalid use of non-static member function" is what is puzzling me. My callbacks are setup how they should be. Any help would be appreciated.

This topic has been closed for replies.