Comparison of rendering times between two kinds image -> (L8_RGB565 and L8_ARBG8888).
Hi,
The same size images, one uses format L8_RGB565 with background colour and the other uses format L8_ARGB88888 transparent background. Two images for screen transition and the L8_ARGB8888 is smoother than L8_RGB565.
Screen2 used L8_ARGB8888 image and add a black box but it's smoother than screen1 used only L8_RGB565 image. How the image render when encounter transparent pixels in the image, the same width and height between two images.
Is it faster to render the same image with a transparent background ?