Skip to main content
Nikunj Patel
Associate III
September 1, 2020
Question

Command to separate the binary from .elf file

Hello @Martin KJELDSEN​ @Community member​ ,@All ALL​ 

We are using TouchGFX based development kit.

  1. STM32F746G-DISCO
  2. STM32F7508-DK

STM32F746G-DISCO :

When we used STM32F746G-DISCO Kit, we are using following command to separate the flash and ext-flash binary.

arm-none-eabi-objcopy.exe -O binary --only-section=*Section "$ STM32F746G_DISCO.elf" ExtFlash.bin;arm-none-eabi-objcopy.exe -O binary --remove-section=*Section "$ STM32F746G_DISCO.elf" Flash.bin

Above Generated binary are working fine and we are loaded using ST-LINK Utility.

STM32F7508-DK :

When we used STM32F7508-DK kit, We are using following command.

arm-none-eabi-objcopy.exe -O binary --only-section=.isr_vector --only-section=.text --only-section=.rodata --only-section=.ARM.extab --only-section=.ARM --only-section=.preinit_array --only-section=.init_array --only-section=.fini_array "$ STM32F7508-DK.elf" Flash.bin; arm-none-eabi-objcopy.exe -O binary --only-section=*Section "$ STM32F7508-DK.elf" ExtFlash.bin;

Above command will create the binary but it is not working fine.

Here, i attached both linker file for both broad, can you please guide me on this point?

Is something that i missed?

Regards,

Nikunj Patel

This topic has been closed for replies.

5 replies

Martin KJELDSEN
Principal III
September 1, 2020

What does "but it is not working fine" mean? Anything more

/Martin

Nikunj Patel
Associate III
September 3, 2020

Hello @Martin KJELDSEN​ ,

It means when i used following command for STM32F7508-DK .

arm-none-eabi-objcopy.exe -O binary --only-section=.isr_vector --only-section=.text --only-section=.rodata --only-section=.ARM.extab --only-section=.ARM --only-section=.preinit_array --only-section=.init_array --only-section=.fini_array "$ STM32F7508-DK.elf" Flash.bin; arm-none-eabi-objcopy.exe -O binary --only-section=*Section "$ STM32F7508-DK.elf" ExtFlash.bin;

It is creating a Two Binary

  1. Flash.bin (0x90000000)
  2. ExtFlash.bin (0x90100000)

When i load both binary using STLINK Utility using External Loader. It will not display anything on display.

Can you please guide me.

Regards,

Kaushal Patel

Tesla DeLorean
Guru
September 3, 2020

Ok, and is flash.bin viable?​

Does your loader​ output any actionable diagnostic information? Like checksumming or hashing what it sees, and that matches the PC side copy?

Does a disassembly show expected code?

Can you run the boot loader in a debugger, and walk the transition into the QSPI image?​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Martin KJELDSEN
Principal III
September 3, 2020

Have you tried debugging? What's the application doing, if anything?

/Martin

Cvega.11
Associate II
September 6, 2020

Hello my friend

Do you know how to use the wifi module (ISM43340-M4G-L44-10 CF) of the stm32h7b3i-dk board?

Any example of a WIFI http server with stm32h7b3i-dk ???