Color problem on stm32h7
- 2 replies
- 480 views
Hello, I am using my custom-developed STM32H7 PCB with an 800*480 TFT display connected via 24bpp RGB. Currently, I am only using external SDRAM (IS42S32800J) for the frame buffer, while my QSPI flash is inactive. For the configuration settings, I based them on the STM32H743I-EVAL board, which I also used as a template.
In the attachment, I shared the color difference issue. Does anyone have suggestions regarding this? Because when viewed with the naked eye, there is a noticeable difference between the tones I designed in TouchGFX and the colors displayed on the screen. Could this be related to the ARGB888 format? Where might I be making a mistake? I have checked all the RGB pins in hardware, and they are all active and working.
The comparative example in the image shows a color tone comparison made with the output taken from the STM32H735 DK.