Associate III
Feb 25, 2026 5:11 AM UTC
Solved
CMD_LIST RAM size for STM32N6
- 3 replies
- 461 views
Hi All,
I'm currently developing a project using an STM32N655. I'm using a 1024x600 px screen. The image format is ARGB8888. Naturally, my frame buffer takes up approximately 2.5 MB. I needed to reduce the size of the CMD list.
My application doesn't have vector graphics or fonts. Can I reduce the size of the CMD list as much as I want? Will this affect performance?
Also, it's not possible to double flash with internal RAM while running a screen of this size. However, would creating frames of different sizes affect the FPS? Currently, the frame rate is 32ms.
Best Regards,
Onur