Skip to main content
Associate
May 4, 2024 1:12 AM UTC
Question

ClickListener Callback Not Working

I have a custom container that has a box inside of it with the ClickListener enabled. I am trying to setup a callback for when the box is clicked. I have the following code setup:

 

 

#include <gui_generated/containers/NavbarBase.hpp>

class Navbar : public NavbarBase
{
public:
 Navbar();
 virtual ~Navbar() {}

 virtual void initialize();

protected:
 virtual void setupMenuItem(TextArea *label, Image *icon);

 virtual void tMenuItemCallbackHandler(const touchgfx::Box &box, const touchgfx::ClickEvent &e);

 touchgfx::Callback<Navbar, const touchgfx::Box&, const touchgfx::ClickEvent&> tMenuItemCallback;

};
#include <gui/containers/Navbar.hpp>


Navbar::Navbar() : tMenuItemCallback(this, &Navbar::tMenuItemCallbackHandler) {

}


/**
 * Adjusts the menu label's X position to be centered with the icon and
 * adjusts the Y position to be centered with the space below the icon.
 * Disabled touch interaction on both elements.
 */
void Navbar::setupMenuItem(TextArea *label, Image *icon) {
	uint16_t labelAdjustedX = icon->getX() + (icon->getWidth() / 2) - (label->getTextWidth() / 2);
	label->setX(labelAdjustedX);
	uint16_t iconBaseY = icon->getY() + icon->getHeight();
	uint16_t labelYPadding = (this->getHeight() - iconBaseY - label->getTextHeight()) / 2;
	label->setY(iconBaseY + labelYPadding);
	label->setTouchable(false);
	icon->setTouchable(false);
}


void Navbar::tMenuItemCallbackHandler(const touchgfx::Box &box, const touchgfx::ClickEvent &e) {
	this->DMenuIcon.setVisible(false);
}


void DMEModeNavbar::initialize()
{
 NavbarBase::initialize();

 // Adjust the positions of the text
 this->setupMenuItem(&this->TMenuLabel, &this->TMenuIcon);
 this->setupMenuItem(&this->DMenuLabel, &this->DMenuIcon);
 this->setupMenuItem(&this->VMenuLabel, &this->VMenuIcon);

 this->TMenuSelector.setTouchable(true);
 this->TMenuSelector.setClickAction(this->tMenuItemCallback);
}

 

 

 

When TMenuSelector is clicked, DMenuIcon should disappear, however, nothing happens. I have looked through a variety of similar posts and code and I do not see what is going wrong here. Any direction would be appreciated. 

This topic has been closed for replies.

3 replies

Associate
May 4, 2024 2:03 AM UTC

Small update: I added a button widget to the project to see how it is configured, when I tapped on the rectangle first and then the button, the rectangle callback would execute...not sure why this is delayed until the button (which was not connected to anything) was clicked...

Graduate II
May 4, 2024 6:27 AM UTC

Hello

Try to invalidate() after set visible false:

void Navbar::tMenuItemCallbackHandler(const touchgfx::Box &box, const touchgfx::ClickEvent &e) 
{
	this->DMenuIcon.setVisible(false);
	this->DMenuIcon.invalidate();

}

About ClickListener, here is good example for box object

https://support.touchgfx.com/docs/development/ui-development/touchgfx-engine-features/mixins

Hope this helps !

Br JTP

ST Employee
Jun 26, 2024 9:11 AM UTC

Hello @jackcampbell ,

Have you tried the solution our amazing friend mentioned? 

Mohammad MORADIST Software Developer | TouchGFX