Skip to main content
KM L.1
Associate III
October 20, 2020
Solved

Changing color of the circle using physical button

Working on designing the GUI in such a way that need​ to change the color of the small circle to indicate the status and also to show the mode changes . If one mode is selected circle color should be green or else white ....... im trying to work on this but im unable to change the color. So if available please send me some examples..

​

​

Thank you

This topic has been closed for replies.
GPa.1
GPa.1Best answer
Associate II
October 22, 2020

Hi!

Try with the following:

Create an interaction for the button with an Action -> Call new virtual function. Generate code and overwrite the function on the ScreenView.

void Screen1View::function1()

{

circle1Painter.setColor(touchgfx::Color::getColorFrom24BitRGB(125, 125, 255));

circle1.invalidate();

}

Don't forget to include:

#include <touchgfx/Color.hpp>

Regards. 

GP

6 replies

GPa.1
GPa.1Best answer
Associate II
October 22, 2020

Hi!

Try with the following:

Create an interaction for the button with an Action -> Call new virtual function. Generate code and overwrite the function on the ScreenView.

void Screen1View::function1()

{

circle1Painter.setColor(touchgfx::Color::getColorFrom24BitRGB(125, 125, 255));

circle1.invalidate();

}

Don't forget to include:

#include <touchgfx/Color.hpp>

Regards. 

GP

KM L.1
KM L.1Author
Associate III
October 22, 2020

Hi,

Thank you for your response!!

I tried with the code you have shared and its working fine as expected.

KM L.1
KM L.1Author
Associate III
October 22, 2020

Can you please help me out in splashing an image for 3 seconds in TFT LCD(the image should display for 3 seconds and then switch back to default screen).

Thank You

Komala

Martin KJELDSEN
Principal III
October 23, 2020

Is this your "splash-screen" ? you could also just have a dedicated screen to display that image, override handleTickEvent() in your view and when 3 seconds have passed, tell the presenter to go to a different screen.

/Martin

KM L.1
KM L.1Author
Associate III
October 26, 2020

Thank you Martin,

Its working fine now .. Thank you for your support.

KM L.1
KM L.1Author
Associate III
October 26, 2020

Hi Martin,

How do I scroll the values using hardware buttons as we are not using touch.

Should I need to use the scrollable container ?