Skip to main content
FTrom
Associate III
February 1, 2022
Question

change the screen in TouchGFX

I m stunding TouchGFX with X-Nucleo-GFX01M1 with an example provided by STm.

In a ScreenView.cpp I can see the following code (Im will copy only one part).

void Screen1View::handleKeyEvent(uint8_t key)
{
 if (animationState != ANIMATION_READY ||
 menuAnimationState != MENU_ANIMATION_READY)
 {
 return;
 }
 
 if (key == '6')
 {
 // Right
 menuSelectRight();

where menuSelectRight is

void Screen1View::menuSelectRight()
{
 menuAnimationState = MENU_ANIMATION_STEP_0;
 menuAnimationTickCounter = 0;
 
 menuAnimationDirectionLeft = false;
}

menuAnimationState is just a enum and menuAnimationDirectionLeft is a boolean.

Can someone expalain where is the function to trig to go in the anohter Screen?

What I found is application().gotoLI found only I found only application().gotoSCREENNAMENoTransition();

It is in Screen1View subclass of Screen1ViewBase whitch call FrontendApplication subclass of FrontendApplicationBase

So I modify the paramter of the class Screen1View that it will read, after many jumps and inherites , from FrontendApplicationBase?

Thanks in advance

Fausto

This topic has been closed for replies.

1 reply

Romain DIELEMAN
ST Employee
February 10, 2022

Hi,

​

Which demo did you base this on ? need a bit more context :grinning_face_with_sweat:. Try to see if there is a GoToScreen interaction set in the Interactions tab in TouchGFX Designer.

​

/Romain