Skip to main content
tv9
Associate
May 7, 2025 7:55 PM UTC
Solved

change the number of data points for when a dynamic graph scrolls over?

Hi,

I'm trying to make a dynamic scroll graph such that the number of data points and x-axis scale changes when a user sets a value through a slider. The issue I'm running into is the inability to update the number of data points for when the graph scrolls (ie if scale is 30 min, then graph scrolls after 30 data points are added; if scale is 10 min, then graph scrolls after 10 data points are added).

tv9_0-1746646798344.png

 

Using the slider below, the user is able to pick a number of minutes between 1 and 30. I already have it so that the slider changes the x-axis scaling and labeling:

tv9_1-1746646822539.png

 

For example, if the slider changes the visible range to 10, the number of data points is still always set to 30. This causes the graph to not scroll until 30 data points have been plotted even if it's not shown on the graph.

tv9_2-1746647120442.png

 

Is there a way to change the number of data points (max capacity) through code? One thing I tried is within the touchgfx framework, I went into the graph widget folder and edited the AbstractDataGraph.hpp to add a setMaxCapacity function, but it doesn't work. Thank you for the help in advance!

 

This topic has been closed for replies.
GaetanGodart
GaetanGodartBest answer
ST Employee
May 8, 2025 11:44 AM UTC

Hello @tv9 ,

 

I don't understand why you are limited.

You already use your slider to set the label so you have a function that does that.

Now you can just "addDataPoint" x times to add x points.

If you want to add one point every second, then just sue the handleTickEvent function and a counter that you increment every tick until you reach 60, then you reset it and add a data point.

 

If my message does not help you, could you share your project and an animation of what you want to achieve?

 

regards,

Gaetan GodartSoftware engineer at ST (TouchGFX)

4 replies

GaetanGodart
GaetanGodartBest answer
ST Employee
May 8, 2025 11:44 AM UTC

Hello @tv9 ,

 

I don't understand why you are limited.

You already use your slider to set the label so you have a function that does that.

Now you can just "addDataPoint" x times to add x points.

If you want to add one point every second, then just sue the handleTickEvent function and a counter that you increment every tick until you reach 60, then you reset it and add a data point.

 

If my message does not help you, could you share your project and an animation of what you want to achieve?

 

regards,

Gaetan GodartSoftware engineer at ST (TouchGFX)
GaetanGodart
ST Employee
May 14, 2025 8:32 AM UTC

Hello @tv9 ,

 

Have you bene able to implement my solution?
If you need extra help I could try to guide you further.

 

Regards,

Gaetan GodartSoftware engineer at ST (TouchGFX)
unsigned_char_array
Lead III
May 14, 2025 8:56 AM UTC

One workaround I can think of if the solution suggested by @GaetanGodart doesn't work is to use interpolation. So always using 30 points. If scale is 10 use 3 times the points.

"Kudo posts if you have the same problem and kudo replies if the solution works.Click ""Accept as Solution"" if a reply solved your problem. If no solution was posted please answer with your own."
tv9
tv9Author
Associate
Jun 3, 2025 4:13 PM UTC

Hi, thanks for the help and sorry for the delayed update! I ended up adding a setMaxCapacity function in AbstractDataGraph.hpp to help set the max number of data points to be shown on the graph.