Skip to main content
Nhor.1
Associate
Apr 18, 2023 6:26 AM UTC
Question

cannot load flash programming algorithm !

Use touchgfx example with stm32f429 discovery Keil with st link usb

When I download it with 2 wire (swd), I get the message cannot load flash programming algorithm. Is there a solution?

(It is the same even if you change the debug option 0x10000000 or 0x20000000. Please help)

This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
Apr 18, 2023 6:32 AM UTC

Can't load it because why?

Can't find it?

Too large to fit in memory?​

The wrong one?

Needs more than one for different memory?

Needs Single or Dual bank?​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..