Skip to main content
HAnh
Associate III
January 9, 2020
Question

Can't program for STM32F746G-DISCO using STM32-ST-Link-Ultility

0690X00000BvoTLQAZ.pngHi Everyone.

I have problem with  STM32F746G-DISCO when i program .hex file demo as link https://www.touchgfx.com/resources/demos/

i'm doing step by step follow in pdf file attached in demo folder.

When i load .hex file in folder "3DBoxDemo" it is OK and run normal.

When i load .hex file in folder "touchgfx_demo2014" it show me a message as "TimeOut" picture. But when i restart STM32F746G-Disco, i see that have program running, but background color is red.

This happen again when i load .hex file in folder "touchgfx_demo2015_480x272_8MB", that mean i see that have program running, but background color is red.

I'm afraid that QSPI chip on STM32F746G-Disco have problem, so that it can't load background.

i hope anyone can help me solve this problem.

Thanks And Best Regards.

This topic has been closed for replies.

17 replies

AVerb.2
Visitor II
October 18, 2021

There is another way to flash the board:

openocd -f board/stm32f746g-disco.cfg -c "program C:/MDK/Boards/ST/STM32F746G-Disco/32F746GDISCOVERY_demo/STemWin/Binary/STM32746G-DISCO_Demo_V1.5.0.hex reset exit"