Skip to main content
Zui
Senior
Jul 12, 2019 7:03 AM UTC
Solved

Can't load "BIG" application on STM32H750DISCOVERY board

When i try to load an application to that disco board i keep having:

An error occured during flash. Please make sure you have the right target connected.

STM32CubeProgrammer is placed in Program Files

STM32CubeProgrammer is placed in Program Files

Converting images

STM32CubeProgrammer is placed in Program Files

STM32CubeProgrammer is placed in Program Files

Flashing bootloader

/usr/bin/sh: C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin\STM32_Programmer_CLI.exe: No such file or directory

gcc/Makefile:463: recipe for target 'flash_bootloader' failed

make[1]: *** [flash_bootloader] Error 127

../gcc/Makefile:53: recipe for target 'flash' failed

make: *** [flash] Error 2

this happen both with my application and the online application downloaded for H750 via touchGfx, but if i make a new project with just a button, it works fine...

should i reinstall stm32CubeMx? (due that error...)

This topic has been closed for replies.
Martin KJELDSEN
Martin KJELDSENBest answer
Principal III
Jul 12, 2019 11:31 AM UTC

You need to install STM32CubeProgrammer

(/usr/bin/sh: C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin\STM32_Programmer_CLI.exe: No such file or directory)

/Martin

8 replies

hansd56
Senior
Jul 12, 2019 7:09 AM UTC

Hi, how big is your program and where do you want to put it?

Zui
ZuiAuthor
Senior
Jul 12, 2019 7:36 AM UTC

as i said, is the online demo.. the one with bathroom and kitchen with no modifications

scottSD
Senior III
Jul 12, 2019 9:34 PM UTC

I have been looking for the source for this demo because I'd like to see how they did the video and have not been able to find it. Could you provide a link to where you found it?

hansd56
Senior
Jul 12, 2019 8:07 AM UTC

I have been able to download it onto a STM32H745I-DISCO with Cube programmer. Same board just with a dual core but addressing the same. You need to select an external loader.

Martin KJELDSEN
Martin KJELDSENBest answer
Principal III
Jul 12, 2019 11:31 AM UTC

You need to install STM32CubeProgrammer

(/usr/bin/sh: C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin\STM32_Programmer_CLI.exe: No such file or directory)

/Martin

Martin KJELDSEN
Principal III
Jul 12, 2019 11:33 AM UTC

If you already have it installed i think, over the last few versions, that the installation folder has changed, and we have a hard reference to the CLI.exe in our Makefile. Just change the path in your makefile to patch your installation if you already have it installed.

/Martin