Skip to main content
EZamo.1
Associate III
Feb 12, 2020 9:51 PM UTC
Question

Can Source code be released for 'Guifw-STM32F4xx-Nucleo.bin' ?

I'm interested in using the Nucleo StmH7 with the L6474 X-NUCLEO-IHM01A1 board.

However I'd like to run STSW-SPIN002 to communicate with it, but that expects to talk to the NUCLEO-F401RE... so I need the protocol that's implemented in order to port to the NUCLEO-H743ZI.

Is it possible to get the source code for Guifw-STM32F4xx-Nucleo.bin?

This topic has been closed for replies.

2 replies

Martin KJELDSEN
Principal III
Feb 17, 2020 9:45 AM UTC

It doesn't sound like it's TouchGFX running on that board, so its definitely not something we've done here at the office. I'll try asking around.

/Martin

EZamo.1
EZamo.1Author
Associate III
Mar 18, 2020 4:04 PM UTC

If the source code that runs on the Nucleo cannot be open-sourced (to be ported to the Nucleo H743ZI) , what about source code for the other side.. the PC software STSW-SPIN002 that talks to it?

If neither, how difficult would implementing the motor movement protocol based on just analyzing the serial traffic between the PC SPIN and the Nucleo F401RE?