Skip to main content
Andrei Chichak
Lead
Jul 16, 2025 11:06 PM UTC
Solved

Can RAM be used for both the display frame buffer and holding dynamic bitmaps?

In my upcoming system I will be needing to use dynamic bitmaps.

Can dynamic bitmaps be located on the same RAM device (say SDRAM on STM32F469 discovery board) that is being used as the frame buffer?

I can carve out a piece of the SDRAM for the dynamic bitmaps, but is the DMA2D going to complain?

Thanks,

Andrei

This topic has been closed for replies.
LouisBBest answer
ST Employee
Jul 17, 2025 10:57 AM UTC

Hello @Andrei Chichak,

If you have enough RAM it shouldn't cause an issue, but you might have some congestion because of a lot of read and write operations on the same bus. Using different memory banks for framebuffers and dynamics bitmap can help to reduce this issue.

BR,

Louis BOUDOST Software Engineer | TouchGFX

1 reply

LouisBBest answer
ST Employee
Jul 17, 2025 10:57 AM UTC

Hello @Andrei Chichak,

If you have enough RAM it shouldn't cause an issue, but you might have some congestion because of a lot of read and write operations on the same bus. Using different memory banks for framebuffers and dynamics bitmap can help to reduce this issue.

BR,

Louis BOUDOST Software Engineer | TouchGFX