Skip to main content
Graduate
Apr 28, 2025 4:44 PM UTC
Question

Can not open an existing TouchGFX project

Hello, 

I'm currently developing a GUI for STM32H747I DISCO as all of a sudden, i couldn't open my touchgfx project properly anymore. Everything worked well before. Now there are no screens shown in the designer and the application name is always "MyApplication" which is not true. Also the Config Icon on the sidebar is often not visible. I also deleted and reloaded the Project into the TouchGFXProjects folder but unfortunately it is always the same problem. My TouchGFX version is 4.24.2. 

I appreciate any help.

Best regards.

This topic has been closed for replies.

2 replies

GaetanGodart
ST Employee
Apr 29, 2025 12:33 PM UTC

Hello @E_SGR ,

 

When you create a project, where is it saved?

GaetanGodart_0-1745929817843.png

 

When you check the folder where the project is saved, can you see it?

 


Also the Config Icon on the sidebar is often not visible.

What is the config button?

 

 


I also deleted and reloaded the Project into the TouchGFXProjects folder but unfortunately it is always the same problem.

What do you mean by deleted and reloaded, do you mean you deleted it and then re created a new project from TouchGFX Designer?

Have you change anything on your PC recently that could be causing the issue?

 

Can you try to upgrade to TouchGFX 4.25.0?

 

Regards,

Gaetan GodartSoftware engineer at ST (TouchGFX)
GaetanGodart
ST Employee
May 15, 2025 11:39 AM UTC

Hello @E_SGR ,

 

Have you been able to move forward on your project?

 

Regrads,

Gaetan GodartSoftware engineer at ST (TouchGFX)