Skip to main content
MThom.2
Associate
July 29, 2020
Question

Can no longer Run Simulator or Run Target

I made a simple demo and was able to run it on my device (STM32H747I-DISCO v(1.0.0)) and I've been able to run it on the simulator. Since then, I've been building up the demo as a concept to show my company and I'm running into compile errors that I can't seem to fix. Here are the compile errors I receive, any help is appreciated!

Run Simulator
 Generate
 Done
 Generate Assets
 make -f simulator/gcc/Makefile assets -j8
 Converting images
 Done
 Post Generate
 touchgfx update_project --project-file=simulator/msvs/Application.vcxproj && touchgfx update_project --project-file=../EWARM/TouchGFX.ewp
 Done
 Compile
 make -f simulator/gcc/Makefile -j8
 Converting images
 Compiling generated/fonts/src/Table_4822485673_60_4bpp.cpp
 Compiling generated/fonts/src/Kerning_4822485673_60_4bpp.cpp
 Compiling generated/fonts/src/CachedFont.cpp
 Compiling generated/fonts/src/Table_verdana_40_4bpp.cpp
 Compiling generated/fonts/src/Table_verdana_20_4bpp.cpp
 Compiling generated/fonts/src/ApplicationFontProvider.cpp
 generated/fonts/src/Table_4822485673_60_4bpp.cpp: In function 'touchgfx::GeneratedFont& getFont_4822485673_60_4bpp()':
 generated/fonts/src/Table_4822485673_60_4bpp.cpp:22:36: error: expected unqualified-id before numeric constant
 static touchgfx::GeneratedFont 4822485673_60_4bpp(glyphs_4822485673_60_4bpp, 0, 60, 0, 4, 1, 0, 0, unicodes_4822485673_60_4bpp, kerning_4822485673_60_4bpp, 63, 0, 0);
 ^~~~~~~~~~~~~~~~~~
 generated/fonts/src/Table_4822485673_60_4bpp.cpp:23:12: error: unable to find numeric literal operator 'operator""_60_4bpp'
 return 4822485673_60_4bpp;
 ^~~~~~~~~~~~~~~~~~
 make[2]: *** [build/MINGW32_NT-6.2/generated/fonts/src/Table_4822485673_60_4bpp.o] Error 1
 simulator/gcc/Makefile:214: recipe for target 'build/MINGW32_NT-6.2/generated/fonts/src/Table_4822485673_60_4bpp.o' failed
 make[2]: *** Waiting for unfinished jobs....
 simulator/gcc/Makefile:176: recipe for target 'generate_assets' failed
 make[1]: *** [generate_assets] Error 2
 simulator/gcc/Makefile:37: recipe for target 'all' failed
 make: *** [all] Error 2
 Failed

And here is my run target

Run Target
 Generate
 Done
 Generate Assets
 make -f simulator/gcc/Makefile assets -j8
 Converting images
 Done
 Post Generate
 touchgfx update_project --project-file=simulator/msvs/Application.vcxproj && touchgfx update_project --project-file=../EWARM/TouchGFX.ewp
 Done
 Compile
 make -f ../gcc/Makefile -j8
 STM32CubeProgrammer is placed in Program Files
 STM32CubeProgrammer is placed in Program Files
 Converting images
 STM32CubeProgrammer is placed in Program Files
 Compiling TouchGFX/generated/fonts/src/Table_4822485673_60_4bpp.cpp
 TouchGFX/generated/fonts/src/Table_4822485673_60_4bpp.cpp: In function 'touchgfx::GeneratedFont& getFont_4822485673_60_4bpp()':
 TouchGFX/generated/fonts/src/Table_4822485673_60_4bpp.cpp:22:36: error: expected unqualified-id before numeric constant
 static touchgfx::GeneratedFont 4822485673_60_4bpp(glyphs_4822485673_60_4bpp, 0, 60, 0, 4, 1, 0, 0, unicodes_4822485673_60_4bpp, kerning_4822485673_60_4bpp, 63, 0, 0);
 ^~~~~~~~~~~~~~~~~~
 TouchGFX/generated/fonts/src/Table_4822485673_60_4bpp.cpp:23:12: error: unable to find numeric literal operator 'operator""_60_4bpp'
 return 4822485673_60_4bpp;
 ^~~~~~~~~~~~~~~~~~
 gcc/Makefile:373: recipe for target 'TouchGFX/build/STM32H747I_DISCO/TouchGFX/generated/fonts/src/Table_4822485673_60_4bpp.o' failed
 make[2]: *** [TouchGFX/build/STM32H747I_DISCO/TouchGFX/generated/fonts/src/Table_4822485673_60_4bpp.o] Error 1
 gcc/Makefile:340: recipe for target 'generate_assets' failed
 make[1]: *** [generate_assets] Error 2
 ../gcc/Makefile:47: recipe for target 'all' failed
 make: *** [all] Error 2
 Failed
 Failed

This topic has been closed for replies.

3 replies

Alexandre RENOUX
Visitor II
July 30, 2020

Hello,

Could you provide the UI code in order to investigate ? It's a problem with the font but I don't know what exactly just from looking at the compiling errors as I don't have any context.

/Alexandre

MThom.2
MThom.2Author
Associate
July 30, 2020

Hi Alexandre,

For some reason if you use Agency FB font, it names the typograph with a bunch of numbers in the code which caused the error. When I use Agency FB Bold it names it AgencyFBBold, so I just switched all my fonts over to that to resolve the issue. It also gets mad if I use in-between sizes like 35, it's like it has to be an even number. (which is probably for rendering fonts the correct size on a embedded display).

Alexandre RENOUX
Visitor II
July 31, 2020

Hello,

Thank you for the feedback. We will look into it.

Glad you found a workaround.

/Alexandre