Skip to main content
Shree
Associate III
Aug 13, 2020 8:36 AM UTC
Question

Can I get TouchGFX + TruyHandsfree demo application source code ?

Hi @Martin KJELDSEN​ ,

1) Is it possible to share the source code for TouchGFX TrulyHandsfree demo ?

https://youtu.be/B8_2XtEK4wk?list=UUPmAQbY9KbHqdQ_GwUGg1bA

2) I am planning to buy STM32F469 Discovery kit for Alexa implementation. Does ST provide Audio codec, Mic etc drivers with this kit ?

Regards,

shree

This topic has been closed for replies.

3 replies

Alexandre RENOUX
Visitor II
Aug 17, 2020 8:58 AM UTC

Hello,

1) For the TrulyHandsFree demo, I'll check if it's possible to share the code and will come back to you.

2) Regarding Audio codec, Mic, drivers, please ask in the corresponding topic as it is not directly related to TouchGFX.

/Alexandre

Shree
ShreeAuthor
Associate III
Aug 28, 2020 12:40 PM UTC

Hi @Alexandre RENOUX​ ,

Did you check if it is possible to share the sensory demo code ?

Regards,

Shree

Alexandre RENOUX
Visitor II
Sep 7, 2020 7:25 AM UTC

Hello,

For the demo shown on the video, most of the graphics are available trough TouchGFX Demo 1 and 2 in TouchGFX Designer. The demo you see on the video is an old one involving 3rd party code.

As for the voice recognition, this cannot be share.

Very sorry for the late answer.

/Alexandre