Skip to main content
m4l490n
Associate III
May 15, 2020
Question

Can I drive a 4-lane mipi display with a STM32H7?

I'm thinking about using a high resolution display like this one

​

​https://www.ebay.com/itm/113385033095

​

But​ I read in the STM32H7 reference manual that it only has two mipi lanes, so my questionis if it is possible to drive a 4-lane display with only 2 lanes, and if possible what would be the impact.

​

Also​, is there a 720x1280 5.5", 6", 7", or 8" display with only two mipi lanes?

This topic has been closed for replies.