Solved
JohanAstrupBest answer
ST Technical Moderator
Jan 8, 2026 1:40 PM UTC
Hello
Which display interface are you planning to use?
It looks like your selected display does not support parallel RGB interface, which is what the TBS available in TouchGFX Designer is configured for. Therefore, you cannot directly replace the display with the current TBS setup.
However, TouchGFX Designer includes TBS examples demonstrating both 8080 and 4-wire SPI display interfaces. I recommend reviewing these examples if you decide to use one of those interfaces.
Best regards,
Johan