Skip to main content
CBoye.1
Associate
Apr 10, 2022 1:44 PM UTC
Question

Can I control a 1bpp, 8 bit parallel ,LCD with LTDC on an STM32H750?

I have spent a couple hours going through the STM32H750 data sheet and haven't been able to come to a conclusion. The display in question is an el.640.200.sk panel that is 1bpp monochrome with a dual 4 bit parallel interface and takes PCLK, VSYNC, and HSYNC. I am wanting to use the LTDC pared with DMA2D as the display has a high refresh rate of 240hz.

So far I have looked at using CLUT with L8 format and leaving pins floating on the 16 bit RGB outputs but it is a huge waste of memory space and gpio pins. Is there a way to configure the LTDC output to 8 bit parallel with the 3 clock/sync signals?

Any help is appreciated.

This topic has been closed for replies.

2 replies

MM..1
Super User
Apr 10, 2022 3:23 PM UTC

LTDC is for 16/24 RGB.

Your LCD maybe can use FMC/FSMC

CBoye.1
CBoye.1Author
Associate
Apr 10, 2022 3:35 PM UTC

That looks promising, cheers. Also, any idea if the graphics library works with it?