Skip to main content
Ikiss.1
Associate II
April 26, 2020
Question

Can any of you give me a small MCU list that i can use without any additional display controller chip for my 5"display ? i would like to use TouchGFX. please see attracted for display data sheet

or i have to use SSD1963 controller no matter what MCU i pick ?

This topic has been closed for replies.

5 replies

berendi
Principal
April 26, 2020

Although any MCU with a LTDC controller would do, I'd recommend the STM32H743 in a package of at least 144 pins (176 if using a 32 bit SDRAM module)

You need the external SDRAM (8 MBytes/64 MBits would do) to hold the framebuffer memory, the internal one is barely enough for displaying simple graphics with a reduced color set, and I'm afraid that the fragmented internal memory map might not play well with touchgfx. Consider adding an external flash module as well if you want to display a lot of graphics. You can use the schematics of the STM32H745I-Discovery board as a reference design.

Ikiss.1
Ikiss.1Author
Associate II
April 28, 2020

Thank you so much, so if i want to go for sure i can use one of the discovery boards as reference design

in my device i would like to have OTA firmware update and been able to generate unique serial number.

is that any MCU have this in one package ?

for serial generation i assume OTP would do it.

Tesla DeLorean
Guru
April 28, 2020

You'll have to write the firmware, but the F4, H7 series have 96-bit UNIQUE ID values, check Reference Manuals

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Ikiss.1
Ikiss.1Author
Associate II
April 28, 2020

yeah but as i see 96-bit UNIQUE ID values pretty difficult to convert/shrink it to actual digestible serial number.

OTP wouldn't it be better ?